The Ultimate Set of Fabrication Tools
They say the best investment is in the tools of one’s own trade. If you are going to invest in the right tools for the job, it only makes sense to take care of your investment. When properly taken care of, most tools will last a lifetime; yet, many people simply toss their tools into the back of their truck where they could potentially get damaged and have a higher probability of getting lost – not anymore.
Finding the right tool for your next tubing job will not be an issue thanks to the Swagelok Tube Fitter’s Toolbox. The toolbox is essential for any job site and contains a complete set of Swagelok hand tools designed specifically for fabricating tubing systems. The set is designed for use with the three most common tube sizes: 1/4, 3/8 and 1/2 inch (outside diameter) tubing. All of the tools are safely and securely contained in a purpose-built, lockable, water resistant Pelican case with wheels to make transporting the toolbox easy.
What's Inside
The Swagelok Tube Fitter’s Toolbox (part number MS-FSTOOLS-KIT) contains the following hand tools:
- Hand Tube Benders – Swagelok hand tube benders provide consistent, high-quality bends in tubing made from materials that can be used with Swagelok tube fittings. The benders for 1/4, 3/8 and 1/2 inch OD tubing are included in the toolbox.
- Tube Cutter – the Swagelok tube cutter cuts stainless steel, soft copper and aluminum tubing from 3/16 to 1 inch outside diameter.
- Tube Deburring Tool – after use of the tube cutter, Swagelok deburring tools deburr stainless steel, steel and hard alloy tube ends.
- Gap Inspection Gauges – Swagelok gap inspection gauges assure the installer or inspector that Swagelok tube fittings have been sufficiently pulled up on initial installation. The gauges for 1/4, 3/8, 1/2, 3/4 and 1 inch fittings are included in the toolbox.
- Tee Wrenches – the tee wrench provides positive backup support when installing Swagelok union tees and crosses, allowing the user to hold the fitting body firmly and precisely. The tee wrenches for 1/4, 3/8 and 1/2 inch fittings are included in the toolbox.
- Pre-Swaging Tools – for Swagelok tube fitting installation in close quarters, the Swagelok pre-swaging tool is a convenient accessory that enables the installer to work in a more open, safe area and complete tube fitting installation by following the retightening instructions. The pre-swaging tools for 1/4, 3/8 and 1/2 inch fittings are included in the toolbox.
- Tube Fitter’s Manual – the indispensable reference, now revised and updated.
The Right Tools Save You Time
You don’t need specialized tools to install Swagelok tube fittings, but our tee and ratchet wrenches do make the job easier and speed up the work. The Swagelok pre-swaging tool, for instance, is another purpose-built tool to ease installation in relatively inaccessible areas. The tool pre-swages ferrules on the tube and allows the installer to complete the installation by following the retightening instructions proving particularly helpful when working in tight spaces, over your head or down by your feet.
Get Yours
Start off the New Year right by organizing and caring for your tools. The case (manufactured by Pelican, one of the most respected brands in tool casing) is also lockable for security, and is equipped with wheels for easy transport. Inside, the foam lining gives each tool its own space, and protects from dirt and debris. No matter how you approach it, the Swagelok Tube Fitter’s Tool Box has got you covered.